Please enter your profile and select news type(s) you want to subscribe to. We’ll start delivering Delta news via email alert after your account being activated.
 
Press Releases
  2016/01/08  
  Innergie Announces New Power Product Line Up for CES 2016
 
  Innergie will unveil its newest power products, including the PowerGear USB-C 45, PowerGear ICE 65, PowerJoy Plus 17, PowerJoy Pro 24, LifeHub Plus and WizardTip at the annual event  
   
Las Vegas – Jan. 7, 2016 – Innergie, a brand of Delta and a leading provider of consumer power products and solutions, has selected the 2016 International CES to expand the company’s power product lines with the additions of the PowerGear USB-C 45, PowerGear ICE 65, PowerJoy Plus 17, PowerJoy Pro 24, LifeHub Plus and WizardTip. These products, in addition to many others from the company, will be on display at the annual event from January 6-9, 2016, in the LVCC, South Hall 1, booth number 21036.

“The Innergie team is dedicated to providing innovative power solutions that consumers can rely on for their various power needs,” stated JJ Chang, Vice President and General Manager of Mobile Power Business Group, Delta. “Whether traveling or living an on-the-go lifestyle, consumers depend on reliable power products to get them through the day. We’re confident our new power products will not only aide them on the go, but will raise the bar in power solutions for years to come.”

Innergie’s PowerGear USB-C 45 is a flexible, forward-looking laptop adapter for Apple’s MacBook and models from other companies with USB-C reversible-plug connector. This adapter embraces USB-C and the thinner, more versatile mobile devices it makes possible. The PowerGear ICE 65 is a universal laptop adapter for the truly mobile lifestyle. Plugging directly into a wall socket, this adapter combines powerful utility with elegant styling, incredible versatility and superb usability. Equipped with interchangeable plugs, it works with the electrical power specifications in over 150 countries around the world.

The PowerJoy Plus 17 is a dual-USB wall charger and is equipped with an embedded smart chip that detects the type of device attached and provides the maximum supported power level, reducing charging time to a minimum. In addition, the PowerJoy Pro 24 features two 2.4A USB ports and smart detection of the type of devices charging, allowing users to power up at top speed. With its dual high-power outputs, it can charge two large tablets at once.

The LifeHub Plus charges multiple mobile devices at once in a smart way. With built-in smart chips, it can detect the type of devices attached adjust power from its three USB ports accordingly. All three ports can deliver 2.4A of output for super-speedy charging, and provide maximum compatibility with USB mobile devices. Lastly, the WizardTip works with Innergie universal laptop adapters to provide users an instant USB port for charging mobile devices at the same time. It is a convenient way to have access to extended capabilities when needed without extraneous bulk.

For more information about Innergie and the company’s various power products, please visit http://www.myinnergie.com.
A three-port mobile super-speed charging hub.
The PowerGear USB-C 45 is a flexible, forward-looking laptop adapter for Apple’s MacBook and models from other companies with USB-C reversible-plug connector.
The WizardTip works with Innergie universal laptop adapters like the PowerGear ICE 65 to give an instant USB port for charging mobile devices at the same time.
News Source: Delta Americas