Please enter your profile and select news type(s) you want to subscribe to. We’ll start delivering Delta news via email alert after your account being activated.
 
Press Releases
  2016/03/11  
  Delta’s LED Lighting Solutions at Light+Building 2016 Frankfurt: A Living Proof of our Superiority in Integrated Smart Monitoring, Energy Efficiency and Power Electronics
 
   
   
Frankfurt, Germany, March 10th, 2016 – Delta Electronics, a leading provider of power and thermal management solutions, introduces today, at Light+Building 2016 Frankfurt, a full range of LED lighting solutions featuring the integration of smart monitoring platforms, industry-leading energy efficiency as well as world-class power electronics technology. The DeltaGrid® communication platform, recently installed to support a 5,000+ LED street light project in Taiwan, provides cloud monitoring functionality to improve maintenance productivity of city-scale street lighting networks. The newly-launched industrial high bay LED lights Staccato series offer industry-leading efficiency of 160 lm/W and wireless connectivity via Zigbee for smart monitoring and control in green buildings and factories.

Our highly diversified spectrum of intelligent LED lighting solutions at Light+Building 2016 Frankfurt will include:

Smart / Remote Monitoring Solution for LED Street Lights: Delta provides a total solution for sustainable cities through the integration of the DeltaGrid® communication platform which collects data locally from high-efficiency LED street lights and tunnel luminaires via the Zigbee wireless protocol and sends it to cloud servers via 3G/GPRS. This system enables real-time status and active failure reporting of city-wide LED lighting networks for better maintenance productivity. In 2015, this proven technology was successfully implemented in a major project in New Taipei City, Taiwan, with more than 5,000 smart LED street lights.

Industrial High Bay LED Lighting: Our brand new wide range of industrial high bay LED luminaires Staccato series boast industry-leading efficiency of up to 160 lm/W and total output from 10,000 lm to up to 30,000 lm. Smart monitoring and control is possible through the integration of 1-10V standard or wireless Zigbee interfaces. The Staccato LED luminaires realize the harmony between reliability, ease-of-installation and lighting aesthetics with their rugged IP66 yet slim design. Being capable of operating under environments of up to 60 degrees Celsius without reducing LED driving current is a key factor in the Staccato series.

LED Driver Solutions: Delta’s programmable LED drivers offer substantial inventory and management costs for customers by easily programing output current. The Constant Light Output (CLO) driver provides the feature to compensate LED’s lumen depreciation which is ideal for applications such as office lighting, warehouse that require constant illuminance. Delta’s CLO driver is designed to service more than 60,000 hours under 40 degrees Celsius ambient environment.

Switching-type Driver-on-Board (SWDOB) LED Light Engine: By leveraging Delta’s core competence in switching power supply, the SWDOB integrates switching-type LED driver and LED light source on the same printed circuit board (PCB) which is a functional architecture for the fabrication of slim and light-weight LED luminaires, especially for commercial applications. Compared to linear-type AC light engines, the SWDOB offers higher efficiency, much wider voltage range as well as flicker-free characteristics.

Delta’s showcase at Light+Building 2016 Frankfurt is located at Frankfurt Messe Hall 4, Level 1, stand K70 between March 13th to 18th, 2016, Frankfurt, Germany.
Delta provides a total solution for sustainable cities through the integration of the DeltaGrid communication platform which collects data locally from high-efficiency LED street lights. This solution was successfully implemented in a major project in New Taipei City, Taiwan, with more than 5,000 smart LED street lights.
Delta provides a total solution for sustainable cities through the integration of the DeltaGrid communication platform which collects data locally from high-efficiency LED street lights. This solution was successfully implemented in a major project in New Taipei City, Taiwan, with more than 5,000 smart LED street lights.
Delta’s brand new wide range of industrial high bay LED luminaires Staccato series boast industry-leading efficiency of up to 160 lm/W, and smart monitoring and control is possible through the wireless Zigbee interfaces.
Delta’s brand new wide range of industrial high bay LED luminaires Staccato series boast industry-leading efficiency of up to 160 lm/W, and smart monitoring and control is possible through the wireless Zigbee interfaces.
News Source: Delta Group